Change Product Line

Camshaft Machining Center with FANUC R-2000iB 'Flying Robots' - Courtesy of TranTek Automation


FANUC Robotics Authorized Integrator TranTek Automation Corporation designed this new automation concept for a series of camshaft machining centers that traditionally used separate linear motion gantry-style pick and place mechanisms and floor conveyors. This new 7th Axis Robotic design, which utilizes FANUC R-2000iB rail-mounted robots, reduces the amount of fixed automation equipment required, cuts four individual automation systems down to one, uses less energy, and frees up floor space while providing capital equipment flexibility.

By integrating these top loader FANUC R-2000iB Material Handling "flying robots" on a overhead rail, separate fixed automation can be removed at each of the CNC machining centers. In the traditional configuration, each machining center had a linear gantry deliver camshafts to and from a conveyor on the shop floor. In this new design, overhead robots pick up and deliver parts from cell to cell. Each movement to the machining center includes removal of a finished part and delivery of a raw part. 

The traditional design also required hundreds of feet of fixed floor conveyors to feed the machining cells. The new configuration by TranTek eliminates the entire conveyor system, freeing up valuable floor space. With the conveyors removed, operators and quality control personnel can move freely around the machine centers. But one of the biggest benefits is capital equipment flexibility. The CNC machining cells can be upgraded or replaced without changing the automation system. Because the FANUC R-2000iB robots can be programmed for variable part positioning, exact machine location and alignment is no longer critical. The manufacturer also has the flexibility to re-use the automation and install a completely different line in the future. 

The FANUC robot programming by TranTek engineers also includes the ability to "park" one robot and use a single robot to feed all machining centers. This feature virtually insures there will be no downtime in the system. All of the engineering, design, and functionality of the system was provided by TranTek Automation. By integrating standard automation products, and by simulating reach studies and cycle times in advance, a faster design/build cycle was accomplished.

Interested in a Robotic Machining Center? Follow the link to request a robot quote, or learn more about our full line of Machining Robots.


Key Technology Demonstrated


FANUC R-2000iB Robot

Machining Robots
  • The slim arm of the R-2000iB and compact footprint allows for increased robot density, increasing throughput.
  • Compact size and ability to flip over and work behind itself maximizes flexibility for work cell design, and saves valuable floor space.
  • Large allowable wrist moments and inertias meet a variety of heavy handling challenges.
  • Non-rotating forearm simplifies hose and cable dressout increasing service life.
  • Proven, reliable FANUC servo drives provide highest uptime and productivity.
  • High-performance motion yields fast cycle times and high throughput.
  < Back to FANUC Robotics Application Case Studies