Change Product Line
     
 

Placing Foam Pads on Insulin Pumps

 
 

A FANUC LR Mate 200iC robot is shown vacuum picking foam pads from a roll and placing them on insulin pumps using iRVision. The camera is mounted directly above the feed slide where a snapshot is taken of the two pads over the red backlight. The foam pads are compared to a fixed position where the robot will move to secure the foam pads. The vision correction offsets the positions used when the foam pads are applied to the pumps.

 
   
     
 

Key Technology Demonstrated

 
 

LR Mate 200 iC Robot

  • Offers maximum performance in a light, efficient, accurate and nimble (LEAN) package
  • Meets the automation needs of a variety of industries including electronics, medical devices, food, metals, plastics, and packaged and consumer goods.  
  • Its compact design and flexibility to quickly adapt to small lot sizes, new styles and other modifications provides manufacturers an affordable solution for small part, flexible production.   
  • The six-axis, LR Mate 200 iC robot rates ‘best in class' for its wrist load capacity, repeatability, work envelope, and speed.
  • Multiple mounting options:  floor, tabletop, inside machines, angle and invert, which maximizes flexibility for small and narrow workspaces.