Tuesday, June 17, 2008
Summer 2008 - FANUC Robotics In the News
The FANUC LR Mate 200iC was recently featured on the cover of Manufacturing Engineering

FANUC Robotics and its integrators are regularly featured in a variety of publications and Websites. The following lists recent articles in the news:


Pharmtech.comRobotics Bring Flexibility to Packaging Operations


Packaging processes, like other pharmaceutical operations, benefit from the speed and repeatability that automation brings. Robotics in particular provide flexibility and accuracy. In some packaging applications such as carton loading, robotics also perform more efficiently than dedicated machines.


Welding Magazine – Robot Training Certification Program


FANUC Robotics America, Inc. now offers a Certified Education Robot Training (CERT) program available to qualified high schools, community colleges and universities.


Assembly Magazine Ensuring Effective Robotic Dispensing


Whether a manufacturer is considering the purchase of a new robotic dispensing system or simply considering converting or upgrading an existing line, there are a number of factors that will determine the project’s ultimate success.


Automotive Design & ProductionAutomation Replacement: Robots (COVER)


As manufacturers are looking for ways to reduce floor space and increase flexibility, robots are being used to replace conventional automation.


Packaging WorldRobots boost cheese productivity


Dutch cheese packager KH de Jong employs robots to depalletize, case-pack, and palletize more than 350 tons of Edam per week.